This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 IPNC Flash nand using CCS出现错误



我通过Arrow-SEED从Appro购买了Davinci TMDSIPNCAM8127,RDK版本为3.5.0,按照其Install Guide使用CCS烧写Nand Flash时出现错误,具体说明如下:

按照文档1.6.1节进行到第7步“Connect Target”时出现错误,

6) Loading and Executing GEL File : After status of A8 is shown as suspended, right click on the core and click on ‘Open GEL A GEL files tab should open in CCS. Right click on the GEL Files window and click on ‘Load GEL…’ Release package contains the gel file IPNC_A8_DDR3.gel at the location <installDir>/Utils/gel. Load this file on A8.
7) Connecting to Host: You will need to connect to the Cortex A8 processor, which is the main host on TI812x/TI814x. Right click on the CortexA8 (Host) core and select ‘Connect Target’.

在Cortex A8 processor上点击右键,选择Connect Target时Cortex A8 processor的状态由(Disconnected: Unknown)变为(Suspended),同时在Console中输出以下错误提示:

CortexA8: GEL Output:
Connecting Target...
CortexA8: Output: **** CENTAURUS2 DDR3 System_Initialisation IS in progress ..........
CortexA8: Output: **** CENTAURUS2 ALL ADPLL INIT IS In Progress .........
CortexA8: GEL: Error while executing OnTargetConnect(): Target failed to read memory at 0x481C5114 at (*((unsigned int *) (Base_Address+0x4))|0x00800000) [IPNC_A8_DDR3.gel:675] at PLL_Clocks_Config((0x481C5000+0x110), CLKIN, N, M, M2, 0x00000801) [IPNC_A8_DDR3.gel:1084] at cmdL3PLL(CLKIN, 19, 800, 4) [IPNC_A8_DDR3.gel:1043] at PLL_SETUP() [IPNC_A8_DDR3.gel:99] at ALL_ADPLL_CLOCKS_ENABLE_API() [IPNC_A8_DDR3.gel:30] at HDVPSSInit() [IPNC_A8_DDR3.gel:21] at OnTargetConnect() .

如下图所示:

不知出现以上问题的原因是什么以及如何解决,谢谢。