配置了DDR_MEM=DDR_MEM_2048M 不就是加载config_2G.bld
但是最后编译出来的u-boot还是只能在1GB上跑,是没有配置生效吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mr. 急急急:
不好意思没有太看明白你的表述。
为什么说编译出来的u-boot只能在1GB上跑?你是有1G和2G的板子吗?
BR,
Eason
你DVRRDK的版本是多少?DDR_MEM=DDR_MEM_2048M 这是在编译的时候,选择使用2G大小的memory配置文件来对linux,代码段以及buffer进行分配。在实使用的时候,你还需要注意uboot的bootargs相关参数的修改。
我有1GB和2GB 的两块板子!我的U-boot已经支持1GB的ddr,现在想要配置u-boot支持2GB的DDR,刚刚接触,不知道怎么配置,求解答!指点一下!