你好,我用了tms320dm6467,但是它外接的24M晶体没有输出?晶体的输出脚电压为0。但是我的另外一块相同设计的板子,24M晶体是正常输出的。我也更换过晶体和dsp,但是都没有效果。我想问下是不是dsp这边有什么特殊设置?或者有什么办法可以判断出来dsp这里没有问题。 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
6467上一共有两个外接时钟,推荐值分别是24M和27M,这两个外部时钟现在我都连接上了现在27M时钟有输出,而24M没有没有输出。负载电容应该没有问题,因为我另一块板子,相同的设计,24M有输出,而且我对比过电容上的静态阻抗,是一致的。我在前面的帖子中貌似看到说是6467有一位寄存器是控制24M时钟的使能的,它的缺省值会使得24M时钟没有输出,我想是不是这个原因。我再问下另一个问题,24M时钟没有的话,JTAG能不能正常工作?
我27M时钟是接到DEX_MXI/DEV_CLKIN(B15)和DEV_MXO上,我24M时钟是接到AUX_MXI/AXU_CLKIN(B17)和AUX_MXO(A17)上,这两个时钟我都外接了。