This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM368 ADC



请教一下,dm368 ADC的采样精度和参考电压时多少呢?谢谢!

  • 你好,

    在DM368的数据手册你可以找到下面的信息:

    6.25 Analog-to-Digital Converter (ADC)
    The device has a 6-channel 10-bit Analog-to-Digital Converter (ADC) interface.

    VDDA18_ADC 1.8-V ADC Supply Voltage

  • 6.25节的;六通道10bit精度的ADC我们都可以看到,也知道1.8的供电电压。但是问的是参考电压。对不起我很无知,请你告诉我,在使用过程中,10bit全1表示多少电压全0表示多少电压?另外控制寄存器中每一位的作用是什么该如何设置?

  • 可以分 享DM368 ADC 的driver code 嗎?, 我目前在 insert adc.ko 會有unknow symbol in module(-1) 的問題. 我用dmesg 得到下面錯誤.

    <4>adc: Unknown symbol proc_create
    <4>adc: Unknown symbol davinci_ioremap_nocache
    <4>adc: Unknown symbol davinci_request_mem_region

    還沒找到方法,解決.