Part Number: TDA4VM
tda4 摄像头驱动接收rgb格式的图片会报错.就是摄像头驱动中配置摄像头的输出图片格式为RGBA或者RGB都会报这个错误

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我把您的问题升级到英文e2e论坛了,因为这周美国感恩节,回复可能会慢些。
请看我们工程师的回复。
Pixel container size in the raw image data structure seems to be incorrect. Can you please make sure that this is set to 16 or less?
When you say RGB or RGMA, what exactly is the pixel format? Is it RAW Bayer format? or RGB output format?
The reason is, the current examples do not support RGB pixel formats. It supports YUV422 or RAW formats.
请看e2e工程师的最新回复。
Which application are you using for capturing RGB format? Please note single camera or multi-camera examples do not support capture of RGB format. In this case, you would require to change the example to change input mipi format.