This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730: DM3730启动异常,老化测试40度下重启测试

Part Number: DM3730
Other Parts Discussed in Thread: TPS65950

Dear Ti team:

         有个问题咨询,关于DM3730CBPA,使用PoP封装 LPDDR+NAND flash ,使用GPMC外挂 32MB的 parallel Nor flash

         在做40度高温老化测试发现部分机器无法启动 ,外观看PCB ,器件,均无短路掉件等异常,测试26Mhz ,32.768Khz 晶振,TPS65950的各路电压,电流均无异常,

          能否从Log信息判断有哪里存在异常,谢谢。操作系统 RTOS, 启动Log如下:

NoLo Version : 2.5.5LOLO-(1)-OMAP3703 0001
NoLo Build : RC_Boot_2.5.5.1
NoLo Compiler: ccintarm
Boot Device : NOR

[10:51:20.063]收←◆Verified.

New NOR Flash Detected

[10:51:20.201]收←◆
Unhandled Exception:
exception mode: abort
fsr: 0x00001848 far: 0x0000098c

**UNRECOVERABLE ERROR**
There was a memory access exception at 0x0000098c of type 'extern fetch1'
this may be due to an access to an invalid memory region,
unaligned access, or a problem with the current memory map.
Please check the memory layout section of your processor manual.
For information about the active memory map type 'info cpu'.

r00: 00000006 r01: 800d8f83 r02: 00000001 r03: 00000000
r04: 00000000 r05: 0000fb4f r06: 8004aae0 r07: 00000006
r08: 000a0001 r09: 4020fc64 r10: 00000001 r11: 0000004a
r12: 8004fc48 sp: 800d8f5c lr: 80010070 pc: 80038964
spsr:60000053 cpsr:600001d7
bt: sp: 800d8ea0 (stack: 800d8000 - 800da000)
(fp:00000000->800d8000, sp:800d8ea0)

谢谢

Best Regards~

x 出现错误。请重试或与管理员联系。