Part Number: TMS320C6748
1.GPIO口内部上下拉电阻阻值大概是多大的
2.当作为输入口使用时,关闭内部上下拉,外部一般需要多大的下拉电阻,可以保证低电平在0.8V以内
3.规格书P79页,±9uA电路如何理解,内部上拉时,电流在70-310uA变化的原因,通过该电流可以计算上下拉电阻吗

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6748
1.GPIO口内部上下拉电阻阻值大概是多大的
2.当作为输入口使用时,关闭内部上下拉,外部一般需要多大的下拉电阻,可以保证低电平在0.8V以内
3.规格书P79页,±9uA电路如何理解,内部上拉时,电流在70-310uA变化的原因,通过该电流可以计算上下拉电阻吗

1. 我这边没有具体的数值,但内部是弱上下拉的。
2. 外部电阻值的选取,请参考数据手册。
4.3 Pullup/Pulldown Resistors
https://www.ti.com/lit/ds/symlink/tms320c6748.pdf
3. 这是漏电流,在文档上有注释。上下拉电阻的阻值选择参考问题2的回复
II applies to input-only pins and bi-directional pins. For input-only pins, II indicates the input leakage current. For bi-directional pins, II indicates the input leakage current and off-state (Hi-Z) output leakage current.
作为输入口时,关闭内部上下拉,漏电流9uA.
打开内部上拉,漏电流70-310uA(忽略9uA), 是否可以推算出上拉电阻大概在10.6K-47K左右
打开内部下拉,漏电流75-270(忽略9uA),是否可以推算出下拉电阻大概在12.2K-44K左右