This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一下各位,我的DM3730的板子共享上nfs的文件系统之后,运行root@beagleboard:/dm3730rootfs/etc/init.d# ./loadmodule-rc start
打印出这样的信息,
FATAL: Module cmemk not found.
FATAL: Module dsplinkk not found.
FATAL: Module lpm_omap3530 not found.
FATAL: Module sdmak not found.
./loadmodule-rc: line 42: amixer: not found
./loadmodule-rc: line 42: amixer: not found
./loadmodule-rc: line 42: amixer: not found
测试例程都用不了了,这该怎么解决呢?
注:我的板子是自带的Angstrom Linux系统。
我手动加载模块# insmod cmemk.ko ,提示如下:
[13244.782775] cmemk: disagrees about version of symbol module_layout
insmod: error inserting 'cmemk.ko': -1 Invalid module format
看了一下板子的内核版本是2.6.32,而.ko文件的版本是2.6.37,应该是版本对应不上,导致无法加载。将DVSDK自带的交叉编译器换成了板子推荐的交叉编译器arm-2009q1/bin/arm-none-linux-gnueabi-gcc,重新执行make demos 编译报错如下:
making package.mak (because of package.bld) ...
js: "./package.bld", line 62: Error: template generation of 'compiler.opt' failed: Error: /usr/local/arm/arm-2009q1/bin/arm-arago-linux-gnueabi-gcc cannot be found. Ensure that rootDir for the GCArmv5T target is set correctly in ./config.bld
gmake: *** Deleting file `package.mak'
making package.mak (because of package.bld) ...
js: "./package.bld", line 62: Error: template generation of 'compiler.opt' failed: Error: /usr/local/arm/arm-2009q1/bin/arm-arago-linux-gnueabi-gcc cannot be found. Ensure that rootDir for the GCArmv5T target is set correctly in ./config.bld
gmake: *** Deleting file `package.mak'
gmake: *** No rule to make target `.configuro'. Stop.
Warning: directory "/usr/local/dvsdk/dvsdk-demos_4_02_00_01/packages" on package path does not exist
js: "/usr/local/dvsdk/xdctools_3_16_03_36/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
make[3]: *** [edge_detection_config/compiler.opt] Error 1
make[3]: Leaving directory `/usr/local/dvsdk/dvsdk-demos_4_02_00_01/omap3530/edge_detection'
make[2]: *** [edge_detection] Error 2
make[2]: Leaving directory `/usr/local/dvsdk/dvsdk-demos_4_02_00_01/omap3530'
make[1]: *** [omap3530] Error 2
make[1]: Leaving directory `/usr/local/dvsdk/dvsdk-demos_4_02_00_01'
make: *** [demos] Error 2
还请指点此种情况该如何解决??多谢!!
这种问题,你还是跟进去看Code、Makefile、Rules.make吧。别人帮不了你。
建议你先把关于环境搭建的文档认真看上一遍。