我想知道tda4芯片的can控制器的基地址是多少芯片手册里面有关于can的RAM, CFG的地址分别是0x40500000和0x40540000不知道该选择哪个?另外基地址选择错误是否会影响控制器接收发器传来的RX信息?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想知道tda4芯片的can控制器的基地址是多少芯片手册里面有关于can的RAM, CFG的地址分别是0x40500000和0x40540000不知道该选择哪个?另外基地址选择错误是否会影响控制器接收发器传来的RX信息?
您好,我们已收到您的问题并升级到英文论坛寻求帮助,链接如下,如有答复将尽快回复您:
e2e.ti.com/.../tda4vm-what-is-the-base-address-of-the-can-controller-on-the-mcu_mcan0-channel
您好,
对于 MCU_MCAN0来说,基地址应该是0x4050000:

您好,
每个模块有3个地址空间:
MCAN Message RAM - MCU_MCAN0为0x4050_0000
MCAN 子系统寄存器- MCU_MCAN0为0x4052_0000
MCAN 内核寄存器- MCU_MCAN0为0x4052_8000
如果您参考 MCAN CSL 示例,即 ti-processor-sdk-rtos-j721e-evm-08_04_00_06/pdk_jacinto_08_04_00_21/packages/ti/CSL/example/mcanEvmLoopback/mcan_evm_app_main_k3.c,则 MCAN的基址为MCAN message RAM。