This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 视频采集接口VPIF使用问题

Other Parts Discussed in Thread: TVP5151, TVP5150

之前发过一个贴,咨询关于利用OMAPL138和TVP5151来实现视频的采集问题,现在每天都在实验,有了一点点的进展,但是问题还是很多,所以还是继续请教高人解答。

简要概述硬件系统:输入信号 PAL制复合视频信号,进入TVP5151后通过 ITU-R BT.656标准(8bit数据线 27MHz时钟线)来同OMAPL138的VPIF接口相连。

TVP5151寄存器配置:配置了0x03地址=0x09(Miscellaneous Controls Register = 0x09),配置了0x28地址=0x04(Video Standard Register = 0x04

之前VPIF的中断服务函数一直进不了,今天实验可以进入。但还有一些问题:

中断问题:

1.在中断中设置了一个计数器,计算中断进入的次数,同时在中断进入后修改数据接收缓存的地址,发现中断进入的次数为5次,然而填写的内容只有3片,后来在中断服务函数中每次修改地址后加入了0.1s的延时,中断次数和输入的数据片数才相同,请问这个是为什么(附上中断服务函数,在asm("nop")处打上断点查看num的值和对应缓存空间DDR2内是否有数据写入)

vpif_isr()
{
     static int num=0;
     VPIF->INTSTATCLR = 0x01;

     if(num > 0)
     {
            VPIF_CAP_CH0-> TLUMA = 0xc1000000+num*(720*288*4);
            VPIF_CAP_CH0-> TLUMA = 0xc1000000+720*288+num*(720*288*4);  
            VPIF_CAP_CH0-> TLUMA = 0xc1000000+720*288*2+num*(720*288*4);
            VPIF_CAP_CH0-> TLUMA = 0xc1000000+720*288*3+num*(720*288*4);

             USTIMER_delay(100000);
     } 
     if(num == 4)
     {
            CLRBIT(VPIF->CH0CTRL, CHANEN);
            asm(" nop ");
     } 

2.VPIF的中断状态寄存器 INTSTAT 的中断标志为什么清除不了,我向INTSTATCLR里写了对应位,但是INTSTAT里的标志依旧存在

传输数据问题:

为什么我收到的一帧图像的TOP帧的亮度和色度值均为0x10或0x01,而BOTTOM帧收到的数据均为0x08。十分不解。附上所配置的VPIF接口代码

VPIF_initReceive()
{
   SETBIT(VPIF->INTENCLR, INT_FRAME_CH0);
   CLRBIT(VPIF->INTEN, INT_FRAME_CH0);
   VPIF->CH0CTRL =0;
   
   VPIF->REQSIZE = 0x20;
   VPIF->EMUCTRL = 0x01;

   VPIF->CH0CTRL = INTFRAME_BOTTOM_ONLY | YCMUX;
   configReceiveVpifRegs(VPIF_CAP_CH0);

   SETBIT(VPIF->INTEN, INT_FRAME_CH0);
   SETBIT(VPIF->INTENCLR, INT_FRAME_CH0);
   
   SETBIT(VPIF->CH0CTRL, CHANEN);
}

configReceiveVpifRegs(vpif_cap_regs_t *vpif_cap_ch)
{
   vpif_cap_ch->TLUMA = 0xc1000000;
   vpif_cap_ch->BLUMA = 0xc1000000+720*288*1;
   vpif_cap_ch->TCHROMA = 0xc1000000+720*288*2;
   vpif_cap_ch->BCHROMA = 0xc1000000+720*288*3;

// 配置BT.656的帧格式数据
   vpif_cap_ch->HCFG = (280 << 16)| 1440;      
   vpif_cap_ch->VCFG0 = (1 << 16)| 23;
   vpif_cap_ch->VCFG1 = (311 << 16)| 313;
   vpif_cap_ch->VCFG2 = (336 << 16)| 624;
   vpif_cap_ch->VSIZE =  625;
   vpif_cap_ch->IMGOFFSET = 720;
}

使用PAL制输入信号,上述的BT.656帧格式配置是否正确

谢谢解答