我现在使用dm648的EVM版,使用的ndk版本是2.0. 用其中的helloworld工程。在EVM板中跑工程24小时内网络不通了。
在函数中
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在使用dm648的EVM版,使用的ndk版本是2.0. 用其中的helloworld工程。在EVM板中跑工程24小时内网络不通了。
在函数中
Chenchu,
#1. 这个文件是与以前版本的例子共用的,对比1.94版本的这个文件,是完全一样的。所以不能因为有这个注释就说是有24hour限制的。
#2. 1.94版本之后的版本就没有24hour的限制了,以前有这个限制是因为production版要收费,现在早就免费开放了,所以也就不再有evaluation版了。
#3. 如果真的存在死机的问题,看看是否打了下面这个链接的补丁:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/ndk/2_00_00/index_FDS.html
#1. 从下面wiki网页说明,2.0NDK不再有评估版。
http://processors.wiki.ti.com/index.php?title=Network_Developers_Kit_Licensing_and_Availability
#2. 下面是NDK的FAQ网页:
http://processors.wiki.ti.com/index.php/Network_Developers_Kit_FAQ
#3. 我有用户用NDK1.94且已量产,要不试一试1.94的版本。
Tony,
我测试了ndk2.1版,在EVM板上可以正常运行。
但我们的方案是SGMII to SGMII 的模式,没有接PHY芯片,直接与博通的交换机芯片的SGMII口相连。我原来修改协议栈,生成新的lib的方案和Network_Developers_Kit_FAQ提到的如下方案相同,如下:
Q: How to properly use the SMA connectors on my DM648EVM board?
If you intend to use the SMA connectors without a PHY then you must perform the two modifications below:
use_SMA_on_port0 = TRUE; use_SMA_on_port1 = TRUE;
pi->TxOn = 0;
Notes:
但是1.92以后的版本都没有cpsw3g_core.c文件了。我想问下如果我仍然想要我们现在的工作方式,我应该对协议栈做哪些修改。否则我们只能换硬件方案了。希望能得到你的帮助,万分感谢!
您好,我们在调试DM648 NDK时遇到问题向您请教一下。 现在使用dm648芯片,使用的ndk版本是ndk_1_92_00_22_eval,用其中的helloworld工程。文档648有两个SGMII口,我们只用了SGMII0,使用的phy芯片是88E1111 –BAB1相连;SGMII1没有用。运行程序后1000M全双工能协商成功,但是ping不通。能否指点一下,谢谢您的时间!