This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AM3359内核电压的问题

Other Parts Discussed in Thread: AM3359

大家好:

       今日在调试AM3359时,在内核启动成功以后,系统不停的在屏幕上打印

       [  132.681566] cpufreq_cpu0: failed to scale voltage up: -22

[  133.288953] cpufreq_cpu0: failed to scale voltage down: -22

开始的时候还是打印这两条提示,后来只打印后面哪一条信息了。

不知怎么解决,希望各位高手帮帮忙了。

  • 在什么板子上调试?

    如果是自己的硬件板,AM335X的供电采用什么方案?

  • 是我自己的板子,电源是TPS65217C,电路与beaglebone-black(BBB)是一模一样的,同样的程序我在BBB和BeagleBone上都跑过,没有发现这个问题,在TI原厂的EVM上也运行过,也没有问题。原理是COPY的,应该没错,PCB我也仔细检查过,也没有问题,系统在打印哪一个字符串时,仍然可以正常工作,各个命令仍然可以运行,不知高手能否帮忙找到问题,谢谢!

  • 如果参考的是BBB的原理图,那现在自己的板子上用的AM335X的芯片是什么版本的?

    在BBB上用的是PG2.0的芯片,与PG1.0在硬件设计上唯一的区别就是NMIn脚

    PG1.0是高有效,PG2.0就改回来了。

  • 我买的是D72版的,是AM3359,不是XAM3359,所以一定是PG2.0版本的。而且我也测量过,NNMI是低电平。不过有一个感觉,似乎AM3359没有找到TPS65217C这个芯片,然后这些内容是AM3359意图设置TPS65217C的时候没有成功的消息。可我仔细校对过原理图和PCB,都没有问题啊。而且其他设备也都能找得到,TPS65217C也能正常工作。莫不是,AM3359与TPS65217C的I2C总线有问题?可是原理肯定没错,PCB走线也十分规整啊。我测试过三块板卡,都是同样现象,匪夷所思,希望大家多多帮助,谢谢Gary Wu 的帮助,也希望大家能帮我搞定这个难题。