Other Parts Discussed in Thread: SYSBIOS
警告信息如下:
<Linking>
warning #10281-D: Section ".bss" requires a STATIC_BASE relative relocation,
but is located at 0x8fcddc34, which is probably out of range of the
STATIC_BASE. STATIC_BASE is located at 0x8fcddc34. Might be required to
correct placement of ".bss" so it lies within 0x8000 of the STATIC_BASE.
warning #10281-D: Section ".neardata" requires a STATIC_BASE relative
relocation, but is located at 0x8fce64f8, which is probably out of range of
the STATIC_BASE. STATIC_BASE is located at 0x8fcddc34. Might be required to
correct placement of ".neardata" so it lies within 0x8000 of the
STATIC_BASE.
warning #10281-D: Section ".rodata" requires a STATIC_BASE relative relocation,
but is located at 0x8fce65d4, which is probably out of range of the
STATIC_BASE. STATIC_BASE is located at 0x8fcddc34. Might be required to
correct placement of ".rodata" so it lies within 0x8000 of the
STATIC_BASE.
warning #10063-D: entry-point symbol other than "_c_int00" specified:
"ti_sysbios_family_c64p_Hwi0"
"edma3_config.c", line 1655: warning #17003-D: relocation from function
"EDMA3_getResourceManager" to symbol "_systemResourceManagerHandle"
overflowed; the 16-bit relocated address 0x8964 is too large to encode in
the 15-bit unsigned field (type = 'R_C6000_SBR_U15_B' (11), file =
"E:\MY_PC\DISK_F\8127\DVRRDK_03.50.00.05\DVRRDK_03.50.00.05\ti_tools\framewo
rk_components\framework_components_3_22_02_08_patched\packages\ti\sdo\fc\edm
a3\lib\release\edma3.ae674<edma3_config.oe674>", offset = 0x00004448,
section = ".text")
warning #10015-D: output file "8147_DVR_RDK_v0350_DSP_20130822.out" cannot be
loaded and run on a target system
'Finished building target: 8147_DVR_RDK_v0350_DSP_20130822.out'
问题:1、这些告警信息是够影响固件的正常运行?
2、产生告警信息的原因是?