在kernel移植到custom的AM1808板上时,遇到标题所示的问题,之后就再也没有任何打印信息了;内核的版本是2.6.37,而且kernel与u-boot,ubl都是出自同一套SDK,我的板子做了些改动,改为从UART 1输出,但是在内核配置make menuconfig时没有找到具体的相关配置项,请问我该如何配置?在终端的输出信息如下:
AM1808 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: NAND
Starting NAND Copy...
Valid magicnum, 0x55424CBB, found in block 0x00000006.
DONE
úNow running in RAM - U-Boot at: c7f5c000
NAND: 256 MiB
MMC: davinci: 0
Bad block table found at page 131008, version 0x01
Bad block table found at page 130944, version 0x01
In: serial
Out: serial
Err: serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
Net: eth_initialize start!
davinci_eth_mdio_enable,clkdiv=56
phy_act_state=0x00000080,pos=54
### main_loop entered: bootdelay=3
### main_loop: bootcmd="nand read.e 0xc1180000 0x600000 0x400000; nboot.e 0xc0700000 0 0x200000; bootm"
Hit any key to stop autoboot: 0
NAND read: device 0 offset 0x600000, size 0x400000
4194304 bytes read: OK
Loading from nand0, offset 0x200000
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2316868 Bytes = 2.2 MiB
Load Address: c0008000
Entry Point: c0008000
## Current stack ends at 0xc7e3bde0 * kernel: default image load address = 0xc0700000
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2316868 Bytes = 2.2 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
kernel data at 0xc0700040, len = 0x00235a44 (2316868)
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
Loading Kernel Image ... OK
OK
kernel loaded at 0xc0008000, end = 0xc023da44
## Transferring control to Linux (at address c0008000) ...
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
U-Boot > pri
EXPORT table = c7fecfa4, htab.size = 521, htab.filled = 11, size = 0
Unsorted: n=11
0: c7e4dbdc ==> ethaddr => 00:00:14:f9:fa:c7
1: c7e4dcf0 ==> stdin => serial
2: c7e4dd50 ==> baudrate => 115200
3: c7e4df48 ==> ethact => DaVinci-EMAC
4: c7e4dfcc ==> bootcmd => nand read.e 0xc1180000 0x600000 0x400000; nboot.e 0xc0700000 0 0x200000; bootm
5: c7e4e1ac ==> bootfile => "uImage"
6: c7e4e4d0 ==> bootdelay => 3
7: c7e4e740 ==> stdout => serial
8: c7e4ec74 ==> ver => U-Boot 2010.12 (Aug 28 2013 - 10:07:15)
9: c7e4eddc ==> bootargs => mem=32M console=ttyS2,115200n8 root=/dev/mtdblock3 rw rootwait
10: c7e4ee24 ==> stderr => serial
baudrate=115200
bootargs=mem=32M console=ttyS2,115200n8 root=/dev/mtdblock3 rw rootwait
bootcmd=nand read.e 0xc1180000 0x600000 0x400000; nboot.e 0xc0700000 0 0x200000; bootm
bootdelay=3
bootfile="uImage"
ethact=DaVinci-EMAC
ethaddr=00:00:14:f9:fa:c7
stderr=serial
stdin=serial
stdout=serial
ver=U-Boot 2010.12 (Aug 28 2013 - 10:07:15)
Environment size: 359/65532 bytes