This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCP NDK



不知道为什么我的帖子发不了,问题都在附件里,麻烦大家看看吧

问题.docx
  • 大家好,我用的是TMS320 674X的芯片,仿真软件为CCS_v5,现在我想用NDK里面的和TCP有关的程序来实现DSP和PC的数据传输,用DaemonNew 回调经过改写过后的 dtask_tcp_echo函数向PC机进行发送数据,里面的send函数是面向连接的。现在我想向PC发4M字节的数,我的和发送数据部分有关的程序 如下:

      for(;;)
        {
           i = (int)recv( s, (void **)recv_buffer, sizeof(recv_buffer), 0);

            // If we read data, start sending until finish
           if(i > 0 )
            {
               while(1)
               {
                   for(j=0; j<2000; j++) {}
                   if(send( s, (void*)xmit_buffer, 2*LEN, 0 ) > 0);
                   {
                       count++;
                   }
                   if(count > back)
                   {
                       break;
                   }
               }
               // if finished sending  wait for next time
               Semaphore_post(sem);
            }
            // If the connection got an error or disconnect, close
           else
               break;
        }

  • recv_buffer 用来接收来自PC端的握手信号,xmit_buffer里面存着待发送的4M字节的数据,问题如下:

    1.dtask_tcp_echa用的是不是TCP协议?

    2.send函数里面有发送的buffer的长度(2*LEN)最大只能设置1024字节,为什么设置大一点就不能发送数据呢?

  • 3.现在我在PC端运行接收程序,发送端每次发送1024字节的数,多次发送,为什么发送小于8次时PC能正确接收到数据,而多于8次时就接收不到数据?
    4.我在每次发送数据之前加了延迟程序,这次能将数据发送到PC机上,可是速度太慢,4M字节的数据用了一分钟才发完。 我试图通过减小延迟时间来提速,但是延迟一减小,数据又发送不出去了?
    请问各位大神,这个问题该怎么解决啊?希望各位不吝赐教!
  • 你好,问下,你用的PHY芯片是什么型号的?