This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: ccs仿真ipc异常

Part Number: AM625


1 使用AM6254官方开发板仿真IPC功能,使用《mcu_plus_sdk_am62x_08_04_00_16》中的ipc_rpmsg_echo_linux程序,在/lib/firmware/目录下替换新编译的am62-mcu-m4f0_0-fw,重新上线后M核运行ipc程序正常,可以看到如下打印信息:
IPC RPMSG ECHO] Dec 15 2022 09:13:26
[IPC RPMSG ECHO] Remote Core waiting for messages at end point 13 ... !!!
[IPC RPMSG ECHO] Remote Core waiting for messages at end point 14 ... !!!

2 使用ccs仿真该工程,发现程序死在了 status = RPMessage_waitForLinuxReady(SystemP_WAIT_FOREVER);这条语句上,理解为M核等待A核将IPC相关的共享内存等内容初始化完成,无法完成后续的仿真

3 一切都使用的是官方默认的硬件和官网的SDK包,其他内容一律没有修改。
4 用ccs仿真其他的程序正常。

能帮忙看看是怎么回事导致的这个现象吗?如果没有ccs仿真功能,程序调试会比较的麻烦。