This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Beaglebone AI插入SD卡后一直刷新eMMC,无法进入SD卡系统

Part Number: AM5728

买了块BBAI,我下载了程序,写入到SD卡。我参考了这一步,并且您希望将映像写入板载 eMMC,您需要按照 http://elinux.org/Beagleboard:BeagleBoneBlack_Debian#Flashing_eMMC 中的说明进行操作,现在插上卡就重新烧录SD,但EMMC的程序都没变,是2020,0406版本的BBB,试了无数次。

Flashing eMMC

To set up the standalone microSD image to automatically flash the eMMC on powerup. Login as debian (password = temppwd) and edit /boot/uEnv.txt with nano (sudo nano /boot/uEnv.txt) or your preferred editor.

In /boot/uEnv.txt:

##enable BBB: eMMC Flasher:
#cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh

Change to:

##enable BBB: eMMC Flasher:
cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh

Optional, update Flasher Scripts:

cd /opt/scripts/
git pull

and reboot the system, it'll flash the eMMC on the next bootup. (make sure to remove the microSD after flashing is complete, otherwise it'll just keep on re-flashing the eMMC)