This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: MCU2_0的中断处理函数一直没被触发?

Part Number: TDA4VM


您好,我们使用主域的gpio0_11做为中断引脚,但是按照下面代码初始化中断后,中断处理函数一直没有被触发。

可以帮忙看看哪里有问题吗?谢谢。

			Intc_Init();
			Intc_IntSetSrcType(11U, (uint32_t)CSL_VIM_INTR_TYPE_LEVEL);
			Intc_IntPrioritySet(11U, 1U, 0U);
			Intc_IntRegister(11U, (IntrFuncPtr) touchIrqHandle, 0U);
			Intc_IntEnable(11U);
			Intc_SystemEnable();

SDK:ti-processor-sdk-rtos-j7-evm-07_03_00_05