This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437中VPFE的缩放器输出



DM6437中VPFE的缩放器输出图像的大小是由限制的么?实际发现宽度必须是16的整数倍,请求确认。

  • 是的,output width 需是16字节的整数倍。

    • Vertical and horizontal resize ratio values (RSZ_CNT.VRSZ and RSZ_CNT.HRSZ) should be within

    the range: 64 to 1024.

    • Output Width:

    – Should be within the maximum limit:

         • width < 1280 (if vertical resize value is in the range: RSZ_CNT.VRSZ = 64 to 512)

         • width < 640 (if vertical resize value is in the range: RSZ_CNT.VRSZ = 513 to 1024)

    – Should be even

    – Should be a multiple of 16 bytes (for vertical upsizing)

  • 缩放器中的YUYV与UYVY的宏设置是颠倒的。