This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6701的DSP运行不稳定



6701的DSP的JTAG有时候连不上有时候连得上,通过HPI口引导时能把程序下到DSP中去,可是当下完程序后置HPI的C寄存器中的DSP_INT位为1以运行DSP时,DSP有时候运行不起来,电源和时钟均正常,总之就是整个DPS不稳定,想请教一下6701的DSP在电路设计上有些什么不一样的要求,比如JTAG脚哪些需要上拉或下拉,上下拉电阻用多大,我现在是按照它的DATASHEET来设计电路的,为什么会不稳定呢?时钟CLK_IN是40MHZ,使用4倍频,输出160M,复位信号也正常。

再想问一下6701的DSP有两种167MHZ的和150MHZ的,核电压分别为1.9V和1.8V,可是我们用的DSP上面标的型号只有***C6701GJC为止,并没有哪里有体现是167,1.9V的还是150,1.8V的,请问怎么区分?

我们还有一批DSP是标明了167,1.9V的,给它上了正确的电压,不稳定的问题依然存在。

总之想请教一下C6701 DSP在电路设计方面是否有什么特殊之处,TI有一个6701开发板的设计是对所有的信号都使用的总线驱动,例如SN74**16244之类的芯片,而我的电路中没有使用,总线驱动是必须的吗?

再补充一个问题,我们使用的6701DSP下载进去程序到它成功运行需要很长的时间(一分多钟),这是什么原因呢?

希望得到您的帮助!

谢谢!