This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678中断问题

在调试状态下,csr、IER寄存器使能相应中断,且IFR中中断置位(中断产生)之后,ISTP的HPEINT没有置位(调试状态下,HPEINT会置位吗?),接下来继续跑程序就会跑飞,请问这是什么状况?我怀疑是cpu处理中断,但是不能正确的找到ISFP地址,所以导致跑飞。

还有就是TMS320C66x DSP CPU and Instruction Set文档中,IST的描述有一段是这样的:

一个ISFP可以包含8到14条指令。这个ISFP包含多少条指令需要在什么地方配置吗?如果超过8条指令的话,32字节的ISFP就存不下这么多指令吧?

8 32-bit instructions in a nonheader-based fetch packet和14structions in a compact header-based fetch packet是什么意思?

我现在写的每个ISFP包含8条指令。