This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm365 resize

Other Parts Discussed in Thread: TVP7002

大家好!

请问一下dm365支持视频的缩放的功能吗?现在要想用dm365 编一个720p的264的编码,然后以任意分辨率(小于720p的分辨率)输出到电视上,是不是要用到resizer的功能呀?

IMP_MODE_SINGLE_SHOT、IMP_MODE_CONTINUOUS 两种模式到底是是什么意思,有什么区别呀?

谢谢!

  • 1. 是的

    2. Video用CONTS

  • 现在用dmai下的resize demo程序(dvsdk_2_10_01_18\dmai_1_21_00_10\packages\ti\sdo\dmai\apps\video_loopback_resize),运行时出现了以下信息

    rsz_dev.users:0

    davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:0:1:108

    davinci_previewer davinci_previewer.2: ipipe_set_preview_config

    davinci_previewer davinci_previewer.2: ipipe_set_preview_config

    vpfe ccdc capture vpfe ccdc capture.1: IMP chained

    vpfe ccdc capture vpfe ccdc capture.1: Resizer present

    vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 576, bpp = 1

    vpfe ccdc capture vpfe ccdc capture.1: hpitch = 720, vpitch = 576, bpp = 1

    Starting ccdc_config_ycbcr...<7>

    starting ccdc_reset...<7>

    End of ccdc_reset...<7>

    Starting ccdc_setwin...<7>ipipe_set_resizer, resizer - A enabled

    DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:

    layer.pix_fmt.bytesperline = 736,

    layer.pix_fmt.width = 720,

    layer.pix_fmt.height = 576,

    layer.pix_fmt.sizeimage =635904

    DavinciDisplay DavinciDisplay.1: pixfmt->width = 720,

    layer->layer_info.config.line_length= 736

    rsz_dev.users:1 //这个是我在内核加的打印,由于这个值不等于 0 导致了下面错误信息的打印

    davinci_resizer davinci_resizer.2:

    mode doesn't allow multiple instances    //这个是内核中的打印

    @10,493,095us: [+7 T:0x4001fd40] ti.sdo.dmai - [Resize] Failed to open /dev/davinci_resizer

    Failed to create resize job

     

    请问哪里出现问题了?导致了Resize_create 创建失败?我在bootagrs已经配置成 CONTS模式,我也试配置成sigle shot mode,但是程序仍然运行不起来,只是提示的错误信息不一样("Operation mode doesn't match with current hw mode")。

    bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.2.42:255.255.255.0:192.168.2.1 root=/dev/nfs nfsroot=192.168.2.67:/home/qinjian/nfs/solo/fs,nolock mem=80M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4 "

     

     

  • 我也遇到了同样的问题,求帮忙分享一下?

    davinci_resizer davinci_resizer.2: Operation mode doesn't match with current hw mode

    vren init ok

    Failed to create resize job

    exit from video render thread begin

    i2c_adapter i2c-0: TVP7002 - clocks per line detected = 216

    End of querystd function.

    vpfe ccdc capture vpfe ccdc capture.1: hpitch = 1280, vpitch = 720, bpp = 1

    vpfe ccdc capture vpfe ccdc capture.1: hpitch = 1280, vpitch = 720, bpp = 1

    Starting ccdc_config_ycbcr...<7>

    starting ccdc_reset...<7>

    End of ccdc_reset...<7>

    Starting ccdc_setwin...<7>ipipe_set_resizer, resizer - A enabled

    video encode buffer size = 1382400

    venc init ok

    writer init ok

  • 这边人水平不行,还是去ti e2e官网问吧