This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有几个关于DDR3L内存芯片的问题。
(1)在BeagleBone开发板上使用了DDR3L芯片。请问一下,在DDR3L的地址线上加上拉电阻(如33欧),再上拉到VTT,是必须的吗?
不是可以通过DDR3内部的ODT,可以实现上拉电阻的效果,而不用外加上拉电阻吗?
(2)我们的嵌入式系统中,对DDR3L进行初始化,应该在U-BOOT中进行吗?还是在U-BOOT之前(即加载u-boot之前)就进行了?
(3)uboot、linux中需要支持DDR3L吗?
谢
1. 关于第一个请参考最新的datasheet中 5.6.2.3 DDR3 and DDR3L Routing Guidelines。
2. 在SPL,也就是MLO中对DDR进行配置。