This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127的Camera interface和Sensor的问题



我们现在在做DM8127高清摄像机的开发。有几个关于Camera interface和Sensor方面的问题想咨询下:

1、DM8127的ISS Module可以通过两个接口接入:并口和CSI2,这里的CSI2指的是MIPI CSI2吗?是遵循这里描述的CSI-2协议吗?http://www.mipi.org/specifications/camera-interface 。因为DM8127文档都没有关于CSI2遵循哪个协议做描述,而且之前我发现CSI-1和CSI-2是不兼容的,所以关于协议匹配性方面现在都谨慎了,请帮忙确认!

2、参考设计用的Sensor是MT9J003,出来的是HiSPi接口,然后通过Lattice的FPGA转成并口,然后再接入DM8127的并口。是因为HiSPi和CSI2不是兼容的?不能直接连?

3、如果第1、2点的都如我所理解的那样,那么如果我们不想用一个FPGA来转接,但是又要达到1080p@60fps的输出(即直接输出1080p@60fps CSI2信号或1080p@60fps 并口信号)。有没什么合适的Sensor可以推荐的?