我们使用的是embest的Devkit 8600开发板,处理器为am3359。在使用中,校准触摸屏之后,触摸屏使用一切正常。但是,每次重启之后,触摸屏会偏移几毫米,方向不定,需要再次重新校准。经检查,每次校准后,/etc/pointercal 文件内容都与之前略有不同。我们分别测了两款触摸屏(7“和8”各一块),都存在此问题。请问,这种情况是否正常,如不正常,应该如何解决?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用的是embest的Devkit 8600开发板,处理器为am3359。在使用中,校准触摸屏之后,触摸屏使用一切正常。但是,每次重启之后,触摸屏会偏移几毫米,方向不定,需要再次重新校准。经检查,每次校准后,/etc/pointercal 文件内容都与之前略有不同。我们分别测了两款触摸屏(7“和8”各一块),都存在此问题。请问,这种情况是否正常,如不正常,应该如何解决?谢谢。
您好,
您问的pclk是指pixel clock么?我们这边分别测试了两块触摸屏,一块是7寸,分辨率800x480,pixel clock是36000000。另一块8寸屏,通过转接板使用LVDS连接,分辨率800x600,pixel clock也是36000000 两款屏幕都存在重启后,触摸屏偏移的情况,其中7寸情况稍好。
tsc方面,都是4线模式。驱动中有个X plate resistance的参数没看明白,没有改动,使用的是原来的200