This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EZSDK 5.02&5.03两个版本里的264编码问题



对High profile的支持是我们使用DM8168方案的一个重要原因。但是在EZDK5.03上,我们遇到了问题,请尽快帮我们解决!

HW:DM8168

SDK:ezsdk5.03

DEMO:capture_encode

I use capture_encode demo. and EZSDK5.3:

tProfileLevel.eProfile = OMX_VIDEO_AVCProfileHigh;

tProfileLevel.eLevel = OMX_VIDEO_AVCLevel42;

eError = OMX_SetParameter (pHandle, OMX_IndexParamVideoProfileLevelCurrent,&tProfileLevel);

but the profile of the  encoded file is baseline profile.

I have tried many profile ,but no one work!!!

//tProfileLevel.eProfile = OMX_VIDEO_AVCProfileBaseline;

//tProfileLevel.eProfile = OMX_VIDEO_AVCProfileHigh;

tProfileLevel.eProfile = OMX_VIDEO_AVCProfileMain;

tProfileLevel.eLevel = OMX_VIDEO_AVCLevel42;

I use this parameter in ezsdk5.2,it works.why?

ezsdk5.03 add many new features and fixed many bugs,we will not use ezsdk5.02 in the future.

在5.03下HP编码出来的视频流用第三方软件测试是BP的,但是参数设置的帧率什么的都是正确的;但是在5.02下用HP编码,HP是正确的,但是帧率什么的是错误的。问下,这两个版本之间的区别及bug。