This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ssd-xds510和C6713开发板连接的问题,必须摁一下reset键才能连接成功!



我用的是ssd-xds510仿真器,开发环境为CCS2.2,开发板是自己仿照一块购买的板子自己制作,与购置的开发板不同的是,我自己做的开发板在14-pin插针和DSP芯片之间没有使用缓冲器,直接连接在一起。

现在连接我自己的DSP开发板时CCS2.2会卡在启动界面,当摁下reset按键的时候才能打开软件界面。而且进入软件界面后必须先reset CPU后再 load program 才能正确运行程序,如果不reset CPU也会造成程序跑飞,没有任何现象。

请各位高手支支招,这几天被仿真器和开发板的连接搞的晕晕的,先谢过!