This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8127+并口AR0331sensor的图象问题



现象:

1.raw_data图象

2.没做白平衡的图象

3.TI白平衡图象

问题:RAW_DATA对吗?

从RAW_DATA来看,实际上有二个方格就曝掉了.一旦通过IE来看,就很明显了.二个方块变为白色了.所以我怀疑RAW_data本身就有问题。

与串口AR0331比较,可知串口版AR0331输出为D0_D13,即14位,而并口数据只有12位,故我在硬件上将Dm8127的D13和D14对地短

路了。并口数据接法,是将AR0331的D0-D11位和DM8127的CAM_D0-CAM_D11位直接相连,反复检测无误。图象曝掉的情况,再调整

光圈时非常明显。请问,这种情况的出现多半是由什么原因引起的?另外图象噪声很大,不干净,很难调到一个满意的结果。