This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于AM3359的DDR3的参数设计

Other Parts Discussed in Thread: AM3359

大家好,我刚刚接触AM3359,板子在DDR3的调试中,遇到了一个问题,希望得到大家的帮助。

DDR3的参数设置中,有两个参数很是奇怪,一个是EMIF_SDCFG,这个参数有没有办法在不使用CCS的情况下计算出来呢,网上的资料我都看了,两个EXCEL工具也都使用了,都没有得到这个参数的计算方法,希望得到各位高手的帮助。还有一个就是PHY_WR_DATA,我在EXCEL工具中的DDR3选项中没找到这个参数啊,在DDR3工具中只有三个参数可以得到,而在DDR2的选项中倒是有四个参数可以得到。

希望大家能够帮帮忙,在不使用CCS和仿真器的条件下如何得到或计算出EMIF_SDCFG和PHY_WR_DATA这两个DDR3的参数。

先谢谢了!

  • 首先感谢您的帮助。这个文档是基本的开发文档,在设计过程中一定会阅读参考的,在设计过程中我反复的查看过该文档。这个文档中,给出了大部分参数的设计方法,但确实没有给出EMIF_SDCFG的设计方法,也没有给出PHY_WR_DATA的设计方法,而且该文档中给出的EXCEL表格中,在DDR3栏中,没有PHY_WR_DATA的参考办法,但在DDR2栏中,就给出了参考办法,感觉很是奇怪。

    参考了论坛中的DDR3设计方法,需要用板子加仿真器得到这两个参考值,能否在不借助仿真器和硬件的基础上得到这个参考值呢,谢谢,盼您帮助。

  • 确实没有给出?请参考链接中的第一条的说明

    SDRAM_CONFIG (@0x4C000008)

  • 非常感谢Gary Wu的帮助。SDRAM_CONFIG这部分我注意过,因为EMIF_SDCFG写入的寄存器就是您给出的提示部分,但是EMIF_SDCFG是一个8位16进制数据,而文档中给出的这些寄存器的组织形式并没有给出(也许是很常用的配置方式,只是我对这部分了解太过粗浅),如果方便,能否告知数据组织形式呢,如何将这14个SDRAM_CONFIG数据组合成为EMIF_SDCFG需要的形式。谢谢。

    另外,我注意到PHY_WR_DATA在DDR2和DDR中的设计算法是一样,但在DDR3栏中确实没有给出方法,请问这个寄存器的设计方法是否参考DDR2/DDR中的设计方法?

    再次感谢Gary Wu的帮助,您的提示给我了很多帮助。

  • 感谢帮助,已经解决