Hello everyone:
1,以太网BOOT:目前在自研板上,C6678的JTAG调试网络通信已经实现,而在使用以太网BOOT模式,使用psendpkt向DSP发送eth文件时,有时候可以成功boot,而有时候无法实现boot,代码中加入了由GPIO控制的LED闪烁代码,发现在BOOT成功时,LED的闪烁有时候正常,而有时候闪烁频率变慢,时钟也检查过,还有可能是什么问题呢?
PS:使用的芯片型号为TMS320C6678CYP...YB2,这个版本应该算是Rev 2.0了吧,还需要预先烧写EEPROM,使用I2C引导加载吗?
2,I2C引导BOOT的疑问:看到资料上所描述,首先是由FPGA将BOOT类型配置为0x0405强制进入I2C BOOT,那么在I2C BOOT成功后,EVM板上的FPGA是通过何种机制去读取SWITCH(GPIO[0-15])的真实状态,从而实现二级BOOT呢?