最近买了广州创龙的OMAPL138的开发板,上边的核心板很小,但是提供的是LINUX2.6.33内核,UBL和UBOOT必须得烧进去NAND FLASH,是不是3.3版本的内核已经支持了UBL和UBOOT直接SD卡启动,上次问了创龙,说3.3内核的要10月底才能整理出来,但是现在比较急,请问谁有可以直接用在广州创龙OMAPL138开发板的3.3内核镜像!有没有大神去移植了?莫非真的要等多20天?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近买了广州创龙的OMAPL138的开发板,上边的核心板很小,但是提供的是LINUX2.6.33内核,UBL和UBOOT必须得烧进去NAND FLASH,是不是3.3版本的内核已经支持了UBL和UBOOT直接SD卡启动,上次问了创龙,说3.3内核的要10月底才能整理出来,但是现在比较急,请问谁有可以直接用在广州创龙OMAPL138开发板的3.3内核镜像!有没有大神去移植了?莫非真的要等多20天?
Tong Tang你好:
我在SD卡中按照TI提供的SD卡格式化方法烧写了AISGEN工具产生的UBOOT文件,能够正常启动,但是发现启动速度较慢,我也在论坛发了帖子
http://www.deyisupport.com/question_answer/dsp_arm/omap_l1x/f/54/t/45741.aspx
后来觉得是否因为我UBOOT.bin太大的原因?之前350k左右,我裁剪了很多东西后压缩到了200k,但是做不到更小了,因为需要支持MMC和UBI等等
那么请问当前RBL的SD卡启动的读取速度大概是多少呢?我SD卡时钟配置为48M,能否有办法获取更高的读写速度呢