Other Parts Discussed in Thread: THS8135
最近真在学习omapl138,刚拿到一块omapl138 lcdk,由于lcdk不板载仿真器,所以需要购买仿真器,由于本人学生一枚,买板子属于个人行为(学校没有款项支持),所以打算买一便宜的仿真器,所以选仿真器上出现了一定的问题,我最开始打算买xds100v2仿真器,但在有些仿真器销售的卖家得到的消息是,xds100v2不完全支持omapl138(好像dsp核可以下,arm支持不是很好),在ti的wiki上找到了一定的资料也是这个观点,所以我想来咨询一下,
问题一:现在的xds100v2的仿真器(不用像下面的那个首先将pll模块从gel提到执行代码中,然后调整频率,最后还检查cpld)能否支持omapl138?
问题二:ti estore上的行吗?
问题三:或者说xds100v3可以吗?
如果大家有其他便宜的仿真器型号提供(学生钱不多,560那种就不要提出来了),欢迎给出,谢谢。
processors.wiki.ti.com/.../XDS100
Q: My XDS100v2 does not work reliabily with the OMAPL138 / DM365 / ARM926 core
- A: This can be caused by a variety of issues such as where the PLL is programmed to the use of Adaptive Clocking emulator. Usually, it is seen as a problem around the PLL setup. This is because the core PLL clock is changing. Example error message:
ARM9: GEL Output: Setup PLL0... ARM9: Trouble Writing Memory Block at 0x1c40900 on Page 0 of Length 0x4: 0x00000004/-2030 @ marker 1026 Error during: Register, Access to an unknown or invalid register was attempted. ARM9: GEL: Error while executing OnTargetConnect(): target access failed.
A couple of things to try:
- Setup the PLL by executing code (ex: UBoot, etc.) instead of using the GEL file. (preferred)
- Turn on adaptive clocking XDS100#Q:_How_can_I_turn_on_adaptive_clocking.3F and setup the timeouts to very slow. In this mode, it is still better to "run" the code and not "step" it.
- Make sure you have the latest CPLD version. To update the XDS100v2 CPLD, please see XDS100#Q:_How_can_I_update_the_CPLD_on_my_XDS100v2.3F