This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657的NDK移植



请教几个问题:

硬件平台:6657,软件平台:CCS5.4,ndk_2_22_02_16

有问题如下:

1、使用EVM板子:client_evmc6657l例程中,程序在什么地方初始化EMAC和PHY的,是不是EVM_init函数中的platform_init函数?

2、针对公司自己设计的板子:外部是一个2端口的PHY芯片,已经把EMAC和PHY调通了(没加NDK),可以用wireshark和DSP收发数据包,怎么样把NDK和EMAC和PHY初始化代码结合起来?

欢迎留言,项目很急,谢谢了