你好: 我使用的ARM是am335x,SD卡启动。文件系统一直可以正常启动。但是今天不知怎么回事,文件系统起来后我想删除一个文件,但是不成功,提示:“Read-only file system”,chmod、mkdir也是如此,内核和uboot我都没变,请问这是什么原因引起的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.SD卡的只读打开了
2.不排除SD卡有问题了,更换SD卡重新做一张启动卡和文件系统
3.看下内核这个地方是否有影响
drivers/mmc/card/block.c文件,去掉只读模式,
static struct mmc_blk_data *mmc_blk_alloc(struct mmc_card *card) {
… /* * Set the read-only status based on the supported commands * and the write protect switch. */
//md->read_only = mmc_blk_readonly(card);
… }