This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

davinci DM8168

您好:

        请问一下:dm8168只有3个硬件编码器,在OpenMax框架中编码最多可以申请多少个VENC组件?可以大于3个么?dn8168编码16路D1视频是怎么实现编码器复用的呢?

  • OPENMAX效率上不适合做多路,如果你想实现该功能,请用DVRRDK软件,已经吧编码器复用的问题给包起来了。

    而且,DM8168的编码器已经很多了,你用这个“只”也太囧了

  • 我想是他理解错了,手册上说的3个编码器是三个硬件编码器,每个硬件编码器支持16通道的数据。

  • 你好向你请教一个问题,8168中的通道(48CH)和采集端口(VIN0_PortA、VIN0_PortB、VIN1_PortA、VIN1_PortB)有什么关系,一直没有理解这两个概念

  • 我的理解是这样的:在选择8位模式时,每个VIN_port就可以分为2个PORT(portA,portB)用,每个port支持16CH输入,所以就48CH。