This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

very large fft例程编译出现的问题



     

vlfft 文件来源:http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/p/12423/67467.aspx

按照Very Large FFT Multicore DSP Implementation Demo Guide.pdf文件中Build Instructions中的描述进行如下设置。

1.把工程放在了下边图片所示位置

2设置环境变量

3.使用6670,修改vlfft Inc文件夹下的vlfftconfig.h文件,将FOUR CORE DEVICE置为1,NUM_CORES_FOR_FFT_COMPUTE 设为4,将VLFFT_16K置为1.

4.从https://gforge.ti.com/gf/project/ctoolslib/frs/?action=FrsReleaseBrowse&frs_package_id=92   上下载STMlib5.0放在路径: C:\STMlib中

编译的时候出现的问题:

在编译之前clean project时候,删除了vlfft_evmc6670l.out文件,但是在编译的时候却无法生成新的vlfft_evmc6670l.out文件。

 

下图是console中的报错描述

问题在哪里,求指导。