This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

deiLink_drv.c: pPrm->inQueParams.prevLinkQueId < pObj->inTskInfo.numQue : failed !!!



Hi

    我在运行run.sh之后,出现以下LOG的内容:

 [m3vpss ]  10460: CAPTURE: VIP0 PortA capture mode is [ 8-bit, Pixel-mux Embedded Sync] !!! 
 [m3vpss ]  10534: CAPTURE: 0: 0xa9500c80, 736 x 288, 00067800 B --> Extra Frames
 [m3vpss ]  10534: CAPTURE: 1: 0xa9568480, 736 x 288, 00067800 B --> Extra Frames
 [m3vpss ]  10535: CAPTURE: 2: 0xa95cfc80, 736 x 288, 00067800 B --> Extra Frames
 [m3vpss ]  10535: CAPTURE: 3: 0xa9637480, 736 x 288, 00067800 B --> Extra Frames
 [m3vpss ]  10535: CAPTURE: 4: 0xa969ec80, 736 x 288, 00067800 B --> Extra Frames
 [m3vpss ]  10535: CAPTURE: 5: 0xa9706480, 736 x 288, 00067800 B --> Extra Frames 
 [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 58 (58)
 [m3vpss ]  UTILS: DMA: 0 of 4: Allocated PaRAM = 58 (0x49004740)
 [m3vpss ]  UTILS: DMA: 1 of 4: Allocated PaRAM = 64 (0x49004800)
 [m3vpss ]  UTILS: DMA: 2 of 4: Allocated PaRAM = 65 (0x49004820)
 [m3vpss ]  UTILS: DMA: 3 of 4: Allocated PaRAM = 66 (0x49004840)
 [m3vpss ] CAPTURE::HEAPID:0    USED:328
 [m3vpss ] CAPTURE::HEAPID:4    USED:20256768
 [m3vpss ]  10542: Assertion @ Line: 1029 in links_m3vpss/dei/deiLink_drv.c: pPrm->inQueParams.prevLinkQueId < pObj->inTskInfo.numQue : failed !!!

 请问是什么原因导致的呢?配置方面?如果是该修改那个参数?

谢谢