This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148EVM音视频不能同时采集的问题?

Other Parts Discussed in Thread: TVP7002

请大家帮忙分析一下:
我使用的DM8148EVM_REV.D       DVRRDK3.0 进行调试
 
我的程序是跑的视频用tvp7002按照720P采集,编码网络发送出去;
如果再启动经行音频采集,视频采集模块会出现问题,出现下面的打印;
如果先经行音频采集,视频采集模块启动失败,程序执行到
System_linkCreate (captureId, &capturePrm, sizeof(capturePrm)); ),
程序就挂了,就可以看到下面的打印。
 
音频采集用程序跑和arecord跑对视频采集的影响效果都是一样的。
 
43824:!!!SLAVE CORE [VPSS-M3] DOWN!!!
SystemLink_copySlaveCoreExceptionContext:146
mmap of [0xbf8e0000:36864]
mmap virt addresss:0x400c0000
munmap of [0x400c0000:36864]
SystemLink_copySlaveCoreExceptionContext:153
[m3vpss ] Unhandled Exception:
[m3vpss ] Exception occurred in ThreadType_Task
[m3vpss ] handle: 0x8ec4da10.
[m3vpss ] stack base: 0x8ef1db00.
[m3vpss ] stack size: 0x8000.
[m3vpss ] R0 = 0x4819c000  R8  = 0x8f0d4d30
[m3vpss ] R1 = 0x000000a0  R9  = 0x8ef25824
[m3vpss ] R2 = 0x00001388  R10 = 0x0000005d
[m3vpss ] R3 = 0x00000001  R11 = 0x00002710
[m3vpss ] R4 = 0x8f0d4c90  R12 = 0x8ef25750
[m3vpss ] R5 = 0x8ef8e6f4  SP(R13) = 0x8ef257e8
[m3vpss ] R6 = 0x0000ffff  LR(R14) = 0x8e127ea7
[m3vpss ] R7 = 0x00000000  PC(R15) = 0x8e19990e
[m3vpss ] PSR = 0x01000000
[m3vpss ] ICSR = 0x0043c803
[m3vpss ] MMFSR = 0x00
[m3vpss ] BFSR = 0x86
[m3vpss ] UFSR = 0x0000
[m3vpss ] HFSR = 0x40000000
[m3vpss ] DFSR = 0x00000000
[m3vpss ] MMAR = 0x4819c028
[m3vpss ] BFAR = 0x4819c028
[m3vpss ] AFSR = 0x00000000
[m3vpss ] Terminating Execution...
 
请大家一起帮忙分析一下,给点建议,谢谢!