This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于用CCS连接OMAP3530调试DSP程序的的问题

Other Parts Discussed in Thread: OMAP3530

各位前人,我想通过CCS5经过仿真器xds100v2来连接使用OMAP3530的c64x+的DSP核,开始的配置是family C6000,variant  OMAP3 -OMAP3530,Connection是xds100v2.ccxml,c64XP_0的gel是系统自动配置的omap3430_c64plus.gel,Cortex_A8_0我给配置的omap3530_cortexA.gel。我仅仅想测试输出一个hello world的小程序,但发现配置好后,我test connection也有问题的,问题是the value is '-342',debug session总是出错,我后来尝试选择ARM核也debug失败!其中提示的错误是:

C64XP_0: Error connecting to the target: (Error -1178 @ 0x6D) Device functional clock appears to be off. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.747.0) 

有两个问题:1.是否CCS5不可以用来连接OMAP3530?可仿真器里面是是有选项的啊?

                        2.是不是我连接的过程中操作有误,但我以同样的方式使用F28335的板子连接,跑程序下载程序调试都没有问题。

 求解答