求助:
我将一个6678配置成SRIO boot模式,并使用另一个6678通过SRIO对其进行加载,程序的加载和运行都没有问题,但是当我们在被加载的程序中加入SRIO的相关代码时,问题出现了:
1、被加载的DSP发出的DIO写无效,DIO读无法完成(completion code始终是0xff)
2、当被加载的DSP开始运行载入的程序之后,其他DSP无法再通过SRIO访问它
这是为什么呢?请高手指教。我们的SRIO代码主要包括:重新配置链路宽度,重启链路,对其他6678进行DIO读写
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求助:
我将一个6678配置成SRIO boot模式,并使用另一个6678通过SRIO对其进行加载,程序的加载和运行都没有问题,但是当我们在被加载的程序中加入SRIO的相关代码时,问题出现了:
1、被加载的DSP发出的DIO写无效,DIO读无法完成(completion code始终是0xff)
2、当被加载的DSP开始运行载入的程序之后,其他DSP无法再通过SRIO访问它
这是为什么呢?请高手指教。我们的SRIO代码主要包括:重新配置链路宽度,重启链路,对其他6678进行DIO读写
请问你的srio boot 模式时,另一DSP(B)是通过直接写IO模式把DSP(A)端的程序加载的么? 如果是,那么DSP(B) 访问是内存地址是多少呀?
能不能把你的程序发给我学习学习吗?