在调试TMS320C6455 与PHY(88E1111)之间的通信时候(通过GMII连接),DSP管脚配置是正确的。运行程序出现NO PHY CONNECT,经过仔细查看,发现是读取 MAC_LIVE 寄存器时候,返回值为0,DSP 认为没有PHY连接。我想问一下,DSP如何检测PHY的存在,然后MAC_LIVE 寄存器 某位置1的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在调试TMS320C6455 与PHY(88E1111)之间的通信时候(通过GMII连接),DSP管脚配置是正确的。运行程序出现NO PHY CONNECT,经过仔细查看,发现是读取 MAC_LIVE 寄存器时候,返回值为0,DSP 认为没有PHY连接。我想问一下,DSP如何检测PHY的存在,然后MAC_LIVE 寄存器 某位置1的。
只要和MDIO通信能有正确回应,应该就不会说no phy
你看看MDIO的连接是否有问题,上面有么有信号;另外,你看看PHY的Address是否和软件里设的一样。如果没有,先改PHY端的address看看,一般是用电阻上下来管脚来决定
你好,你这个PHY芯片驱动能不能给我发一份,我的换了芯片,不想读手册,急需,我只要库文件就行了,谢谢,1016498692@qq.com