自己做的C6672板子( TMS320C6672CYP-YB20 ),在CCS5.3环境下使用spectrum的XDS560V2仿真器。连接双核没有问题,但在调试时,核0的程序经常跑飞,终止程序运行时,CCS报错
C66xx_0: Trouble Halting Target CPU (Error-1060@0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e. g. lower TCLK). (Emulation package 5.0.872.0)
我已经把主频降到300M 了也还是这个现象,电源方面使用了TI的UCD7242和UCD9222、TPS65251 TPS51200,电源一切正常,GEL文件是我通过6678GEL自己修改的,不知道和GEL有没有什么关系
希望大家帮忙看看有什么好的解决办法,非常感谢各位