This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 SATA hard resetting link

我现在用的是DVRRDK3.5 和DM8168

在系统开机的过程中,kernel打印如下信息:

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata1.15: Port Multiplier 1.2, 0x197b:0x0325 r0, 5 ports, feat 0x5/0xf

ata1.00: hard resetting link

ata1.00: failed to resume link (SControl 0)

ata1.00: SATA link down (SStatus 0 SControl 0)

ata1.01: hard resetting link

ata1.01: SATA link up 3.0 Gbps (SStatus 123 SControl 320)

ata1.02: hard resetting link

ata1.02: failed to resume link (SControl 0)

ata1.02: SATA link down (SStatus 0 SControl 0)

ata1.03: hard resetting link

ata1.03: failed to resume link (SControl 0)

ata1.03: SATA link down (SStatus 0 SControl 0)

ata1.04: hard resetting link

ata1.04: failed to resume link (SControl 0)

ata1.04: SATA link down (SStatus 0 SControl 0)

ata1.01: ATA-8: ST2000DM001-9YN164, CC4B, max UDMA/133

ata1.01: 3907029168 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata1.01: configured for UDMA/133

ata1: EH complete

scsi 0:1:0:0: Direct-Access     ATA      ST2000DM001-9YN1 CC4B PQ: 0 ANSI: 5

sd 0:1:0:0: Attached scsi generic sg0 type 0

sd 0:1:0:0: [sda] 3907029168 512-byte logical blocks: (2.00 TB/1.81 TiB)

sd 0:1:0:0: [sda] 4096-byte physical blocks

sd 0:1:0:0: [sda] Write Protect is off

sd 0:1:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

 sda: sda1 < sda5 >

sd 0:1:0:0: [sda] Attached SCSI disk

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata2.15: Port Multiplier 1.2, 0x197b:0x0325 r0, 5 ports, feat 0x5/0xf

ata2.00: hard resetting link

ata2.00: failed to resume link (SControl 0)

ata2.00: SATA link down (SStatus 0 SControl 0)

ata2.01: hard resetting link

ata2.01: SATA link up 3.0 Gbps (SStatus 123 SControl 320)

ata2.02: hard resetting link

ata2.02: SATA link up 1.5 Gbps (SStatus 113 SControl 320)

ata2.03: hard resetting link

ata2.03: failed to resume link (SControl 0)

ata2.03: SATA link down (SStatus 0 SControl 0)

ata2.04: hard resetting link

ata2.04: failed to resume link (SControl 0)

ata2.04: SATA link down (SStatus 0 SControl 0)

ata2.01: ATA-8: WDC WD10EALX-089BA1, 19.01H19, max UDMA/100

ata2.01: 1953525168 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata2.01: configured for UDMA/100

ata2.02: ATA-8: WDC WD20EARX-00PASB0, 51.0AB51, max UDMA/133

ata2.02: 3907029168 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata2.02: configured for UDMA/133

ata2: EH complete

 

 

系统起来后,挂载的硬盘可以正常工作。

 

但是这些打印非常影响开机速度,它们大概需要二三十秒才能打完。

 

从打印信息看,它们并没有对硬盘驱动决定作用。想试图disbale检测,不知道怎么去关闭?

还请高人指点!