This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm642功耗问题

Other Parts Discussed in Thread: TPS54310

公司用贵公司TMS320DM642AZDK6芯片,发现发现我们整块板子都非常烫,板子大小6CM*8CM的。现在可以确定买的芯片肯定是原装的,以前设计时用的贵公司TPS54310芯片也是很烫,现在用的令一款芯片。同样很烫。其实我们的产品从功能上都已经实现了,就是老是重启,我怀疑和温度有关系,上周我们请教了贵公司代理商新晔电子点技术支持,还是没说出问题所在。希望得到贵公司的帮助

 上海泰易电子 朱兴旺 021-56980928

  • 请您先检查一下上电时序是否正常,是否依据数据手册规定;电流是否稳定,包括复位的程序。

  • 这个我们也查看了最新的手册,现在的芯片上电没有时序问题了,也就是说3.3V电压和1.4V电压可以同时上电,以前公司电源用的TPS54310做的,发现温度也是比较高,后改了成本更低的AOZ1017做饿,电压电流应该满足条件。

    电流温度怎么看啊, 至于说复位的程序,我们板子能正常工作了,就是稳定性不行。还是就是温度高,想了解怎么引起的

  • 电流的话你可以用显示电流的电源或者串个电流表在电源和板子之间,温度,有专门测的,用一个探头的那种。DM64X的最大电流有1A的,不知道你用的什么频率,很多芯片像FPGA,DDS,功放更不用说,有70多度,摸着会烫手。如果你整块板子都烫,那就要检查电路设计了。