This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 blackhawk 连接不上



我使用的是TMDXEVM6678和CCS 5.2.1,在连接的时候,按照正常的亮灯顺序,应该是绿灯亮,然后黄灯和红灯亮。
但是我现在上电,绿灯亮后,只有红灯亮,黄灯没有反应。而且,我现在也没有处于安全模式。
测试连接时,输出如下:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\ADMINI~1\AppData\Local\.TI\213602635\
0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
The library build date was 'May 30 2012'.
The library build time was '23:17:26'.
The library package version is '5.0.747.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-100' (0xffffff9c).
The title is 'SC_ERR_BAD_GENERIC'.

The explanation is:
The controller or software detected an error with an unknown cause.
This error number is used when detailed information is not available.

[End]

请问,现在应该如何才能连上板子呢??
谢谢!