Other Parts Discussed in Thread: TMS320C6678
附件中是新手入门CCSV5调试TMS320C6678笔记,带工程源文件与调试笔记
发现在程序单步进入到delay子函数时,子函数中的i变量被多减了1
是否正确与原因,希望网友们验证
此帖于2011年12月11日已经更新,入门笔记中增加了,用多个核调试同一个程序的笔记,希望可以对入门的新手有用!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C6678
附件中是新手入门CCSV5调试TMS320C6678笔记,带工程源文件与调试笔记
发现在程序单步进入到delay子函数时,子函数中的i变量被多减了1
是否正确与原因,希望网友们验证
此帖于2011年12月11日已经更新,入门笔记中增加了,用多个核调试同一个程序的笔记,希望可以对入门的新手有用!
HI Jack:
你好:
我首先新建了一个工程,在工程里添加了三个文件,分别为:link.cmd ,boot.asm ,main.asm。link.cmd 里的内容如下:
--entry.point=RESET_RST
MEMORY
{
CEO: o=0X80000000 l=0x10000000
L2SRAM:o=0X00800000 l=0x0000fc00
}
SECTIONS
{
.myboot > L2SRAM
.my program >L2SRAM
.cinit >L2SRAM
.pinit >L2SRAM
.text >L2SRAM
.stack >L2SRAM
.bss >L2SRAM
.const >L2SRAM
.date >L2SRAM
.far >L2SRAM
.swith>L2SRAM
.sysmem >L2SRAM
.stack >L2SRAM
.tables >L2SRAM
.cio >L2SRAM
}
boot.asm 的内容如下:
.sect ".myboot"
.ref start
.global RESET_RST
RESET_RST:
MVKL .S2 start ,B3
MVKH .S2 start ,B3
B .S2 B3 ;跳转的main
NOP
NOP
...(多个NOP)
RESV1:(多个NOP)
RESV2:(多个NOP)
..........:
INT15:(多个NOP)
mian.asm 的内容如下:
.sect ".myprogram"
.global start
start:
.......(给A0~A15,B0~B15写0)
MVC TSR ,B0
OR B0,0x00000001,B0
MVC B0,TSR ;给TSR.GIE 写1
MVC.S2 CSR,B9
OR.S2 B9,0X00000001,B9
MVC.S2 B9,CSR ; 给CSR.GIE 写1
MVKL 0X00000203,B1
MVC B1,IER ;使能9号中断
MVKL 0X00000200,B1
MVC B1,ISR ;设置9号中断
NOP 2 ;这里应该开始跳转到IST
MVC IFR,B4
NOP 5
所有程序都在这里,可以成功生成.out 文件,当我选择 C6678 Device Funtional simulator ,little Endian ,加载.out 文件时,可以正常跳转到9号中断,但当我选择Blackhawk xds560v2-USB mezzanine emulator 时,连接上C6678板子,加载.out文件时,则始终不能跳转到9号中断,不知道为什么?TSR.INT 位始终为0,如能指点一二,不甚感激!
jasom您好,
请问你在EVM板测试新建cxml文件时,有没有选择相应的6678.gel文件?具体在EVM板子上的测试流程请参考https://www.deyisupport.com/question_answer/f/53/t/4899.aspx附件中01 Intro to CCCSv5.pptx关于新建工程如何在EVM板上测试的说明。谢谢!