This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 输入晶振选择

OMAPL138 输入晶振 我用的是有源晶振,设计的时候用的是3.3V的晶振,输出LVTTl电平。现在板子电流越来越大,又看了TI的文档,说是晶振需要1.2V的。是不是因为我的晶振电平大的缘故把片子弄坏了?

如果使用有用晶振,必须用1.2V的吗?一般晶振没有1.2V的怎么办?

如果只要了3.3V,OMAPL138的引脚DVDD18 还是必须接上1.8V吧?如果不接能出现什么问题?

谢谢!!

  • OMAPL138的时钟输入电平为1.2V,可以用3.3V的晶振输出经过电阻(选择100多ohm的电阻)分压得到1.2V的时钟信号。

    板子电源越来越大能确定是不是这个问题造成的。建议你测量一下其它供电电平是否正常。

    这句话是什么意思呢?

    如果只要了3.3V,OMAPL138的引脚DVDD18 还是必须接上1.8V吧?如果不接能出现什么问题?