This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6713带BIOS时,如何使用中断(CCS3.3)



环境:CCSV3.3 ,DSP/BIOS 5.41.10.36

现象:建立了BIOS,能够实现LOG_printf();现在想要实现定时器1的中断控制LED灯的闪烁,将该中断映射到INT15,在BIOS中对HWI_INT进行设置,函数名为_Timer1_int15();有中断服务程序;但是在中断里面设置断点,发现没有进中断。

请问:在使能中断时还能够用IRQ_enable()这个函数么?如果可以的话,还有什么地方需要设置呢?另外,使用DSP/BIOS之后是不是应该有一个real Time运行的选项呢?我在运行时发现该选项为灰白,不能选择。

望各位专家指导!