This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于c5509a芯片的替换及后续产品的问题

您好,Shine

先把我的问题简单的描述下, 我们项目中有2块板卡,前端板卡是c5509a的数据采集卡,后端板卡是数据处理板卡(ARM, 带spi接口),c5509的bootloader是通过ARM下载进去的,现在我们的问题在于通过什么方式把5509的bootloader下载到c5509a。之前做过很多的前期预研,也问过相关问题,http://www.deyisupport.com/question_answer/dsp_arm/c5000/f/48/t/48376.aspx,现在还想在想些更稳定可靠地方法。

有几个问题想请教下:

1. 请问有没有对c5509a芯片pin-pin兼容的后代产品,能替代5509a,下载方式能用通用接口,能比较容易的解决我上述问题的芯片?

2.  在5509a-bootloader里面,spi下载中,spi的时钟是根据DSP input clock period来的,我们板卡c5509a的晶振是12M, 换算下来SPI 的时钟是50K, 实际量到的也是50K, 我的问题是dsp input clock period 是哪里的时钟? 如何提高SPI下载的工作时钟?

万分感谢!