最近用DM642做X264的移植,在CCS3.3下进行软仿真,载入.OUT后,运行到编码完YUV视频后出现“Error: Memory Map Error: READ access by CPU to address 0x10101000, which is RESERVED in Hardware.”本应输出的.264文件也出不来了。连上硬件后,同样也是错误,但变成了“Error: Error 0x0000000C/-2044 Error during: Register, Break Point, No breakpoint at 0x10F0000C Sequence ID: 16 Error Code: -2044 Error Class: 0x0000000C”RESET CPU也没用,都是无法输出文件。请问这该怎么解决啊?